AXIS#.PL.OFFSET

Description

This parameter sets an offset that is applied to AXIS#.PL.FB.

Examples

The position feedback is at 1000 [deg]. AXIS#.PL.OFFSET is set to 500. The new position feedback is 1500 [deg].

-->AXIS1.PL.FB
1000.000 [deg]
-->AXIS1.PL.OFFSET 500 -->AXIS1.PL.FB 1500.000 [deg]

Versions

Action Version Notes
Implemented 02-01-04-000  

General Information

Type Read/Write
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value

0 counts

Note: Default is adjusted to account for the units selected by the user.

Data Type Float
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
AXIS1.PL.OFFSET

500ch

13h

Signed32

Position

-

Read/Write

No

AXIS2.PL.OFFSET

510ch

13h

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.OFFSET

5917

171D

Signed32

Read/Write

Position

AXIS2.PL.OFFSET

71453

1171

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.OFFSET

5917

Signed32

Read/Write

Position